Is there any significant current that flows into the SDA/SDC or INT pins if they are powered (say a 2kohm pull-up to 3.3V) while the rest of the DS125DF410 is powered down (Vdd = 0V)?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is there any significant current that flows into the SDA/SDC or INT pins if they are powered (say a 2kohm pull-up to 3.3V) while the rest of the DS125DF410 is powered down (Vdd = 0V)?
No, there should not be. Per datasheet the current for these pins is only in the microamps range.
|
3.3 V LVCMOS DC SPECIFICATIONS (SDA, SDC, INT) |
|||
|
VIH High Level Input Voltage |
VDD = 2.5 V |
1.75 3.6 |
V |
|
VIL Low Level Input Voltage |
VDD = 2.5 V |
GND 0.7 |
V |
|
VOL Low Level Output Voltage |
IPULLUP = 3 mA |
0.4 |
V |
|
IIH Input High Current |
VIN = 3.6 V, VDD = 2.5 V |
20 40 |
μA |
|
IIL Input Low Current |
VIN = GND, VDD = 2.5 V |
–10 10 |
μA |
|
fSDC SMBus clock rate |
Slave Mode |
100 400 |
kHz |
|
Master Mode (5) |
400 |
kHz |
|
Cordially,
Rodrigo Natal
HSSC Applications Engineer