Please recommend an IC that can implement the function of the block diagram above.
I want to transmit a 6 pin signal (consisting of Digital Audio signal, UART signal and GPIO signal) as 1 signal.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Please recommend an IC that can implement the function of the block diagram above.
I want to transmit a 6 pin signal (consisting of Digital Audio signal, UART signal and GPIO signal) as 1 signal.
You need at least two wires, for the signal and ground. And the transformations you are describing are called "serializing" and "deserializing".
It would be a better idea to run six wires between the boards. In fact, at 3 m, it's likely that you need differential transmission (e.g., LVDS), so you would need eleven wires.
Hansook,
Along with what Clemens said, our group doesn't have a transceiver that can do this. We have LIN and IO-Link devices that has a single-ended communication bus, but these won't be able to combine 6 signals into one bus signal (I believe that's what is trying to be done here).
Can you elaborate a bit more on else is trying to be done here?
Regards,