Part Number: TIC12400-Q1
Other Parts Discussed in Thread: TIC12400,
I am using tic12400 with c2000. I am able to read device id but when I am trying to write a register and read it back then result is not as expected. I am attaching the code. Thanks for the help in avance.
//#############################################################################
//
// FILE: spi_ex4_eeprom.c
//
// TITLE: SPI EEPROM
//
//! \addtogroup driver_example_list
//! <h1>SPI EEPROM</h1>
//!
//! This program will write 8 bytes to EEPROM and read them back. The device
//! communicates with the EEPROM via SPI and specific opcodes. This example is
//! written to work with the SPI Serial EEPROM AT25128/256.
//!
//! \b External \b Connections \n
//! - Connect external SPI EEPROM
//! - Connect GPIO8/SPISIMO on controlCARD (GPIO16 on LaunchPad) to external
//! EEPROM SI pin
//! - Connect GPIO9/SPICLK on controlCARD (GPIO56 on LaunchPad) to external
//! EEPROM SCK pin
//! - Connect GPIO10/SPISOMI on controlCARD (GPIO17 on LaunchPad) to external
//! EEPROM SO pin
//! - Connect GPIO11/CS to external EEPROM CS pin
//!
//! \b Watch \b Variables \n
//! - None
//!
//
//#############################################################################
// $TI Release: F28004x Support Library v1.11.00.00 $
// $Release Date: Sun Oct 4 15:49:15 IST 2020 $
// $Copyright:
// Copyright (C) 2020 Texas Instruments Incorporated - http://www.ti.com/
//
// Redistribution and use in source and binary forms, with or without
// modification, are permitted provided that the following conditions
// are met:
//
// Redistributions of source code must retain the above copyright
// notice, this list of conditions and the following disclaimer.
//
// Redistributions in binary form must reproduce the above copyright
// notice, this list of conditions and the following disclaimer in the
// documentation and/or other materials provided with the
// distribution.
//
// Neither the name of Texas Instruments Incorporated nor the names of
// its contributors may be used to endorse or promote products derived
// from this software without specific prior written permission.
//
// THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
// "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
// LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
// OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
// SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
// LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
// DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
// THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
// (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
// OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
// $
//#############################################################################
//
// Included Files
//
#include "driverlib.h"
#include "device.h"
#include "stdio.h"
//
// Defines
//
#define EEPROM_ADDR 0x0000
#define NUM_BYTES 8
//
// SPI EEPROM status
//
#define MSG_STATUS_READY_M 0x0001 // EEPROM is ready (not busy)
#define MSG_STATUS_WRITE_READY_M 0x0002 // EEPROM
#define MSG_STATUS_BUSY 0xFFFF // EEPROM is busy (internal write)
//
// Opcodes for the EEPROM (8-bit)
//
#define RDSR 0x0500
#define READ 0x0300
#define WRITE 0x0200
#define WREN 0x0600
#define WRDI 0x0400
#define WRSR 0x0100
//
// Defines for Chip Select toggle.
//
#define CS_LOW GPIO_writePin(11, 0)
#define CS_HIGH GPIO_writePin(11, 1)
//
// Globals
//
uint16_t writeBuffer[8] = { 0x00, 0x01, 0x02, 0x03, 0x04, 0x05, 0x06, 0x07 };
uint16_t readBuffer[8] = { 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00 };
uint16_t rx_buff[2];
uint16_t i = 0;
uint16_t parity = 0;
//
// Function Prototypes
//
void initSPI(void);
uint16_t readStatusRegister(void);
void writeData(uint16_t address, uint16_t * data, uint16_t length);
void readData(uint16_t address, uint16_t * data, uint16_t length);
void enableWrite(void);
void spi_write(uint32_t address, uint32_t data);
void spi_read(uint32_t address);
//
// Main
//
void main(void)
{
// uint16_t error = 0;
// uint16_t i;
//
// Initialize device clock and peripherals
//
Device_init();
//
// Disable pin locks and enable internal pullups.
//
Device_initGPIO();
//
// Initialize GPIOs 8,9,10,11 (16,56,17,11 on LaunchPad)
// for SPISIMO, SPICLK, SPISOMI, CS respectively
//
GPIO_setPadConfig(DEVICE_GPIO_PIN_SPISIMOA, GPIO_PIN_TYPE_PULLUP);
GPIO_setPinConfig(DEVICE_GPIO_CFG_SPISIMOA);
GPIO_setQualificationMode(DEVICE_GPIO_PIN_SPISIMOA, GPIO_QUAL_ASYNC);
GPIO_setPadConfig(DEVICE_GPIO_PIN_SPICLKA, GPIO_PIN_TYPE_PULLUP);
GPIO_setPinConfig(DEVICE_GPIO_CFG_SPICLKA);
GPIO_setQualificationMode(DEVICE_GPIO_PIN_SPICLKA, GPIO_QUAL_ASYNC);
GPIO_setPadConfig(DEVICE_GPIO_PIN_SPISOMIA, GPIO_PIN_TYPE_STD);
GPIO_setPinConfig(DEVICE_GPIO_CFG_SPISOMIA);
GPIO_setQualificationMode(DEVICE_GPIO_PIN_SPISOMIA, GPIO_QUAL_ASYNC);
GPIO_setPadConfig(11, GPIO_PIN_TYPE_PULLUP);
GPIO_setPinConfig(GPIO_11_GPIO11); //GPIO_11_SPIA_STE);
GPIO_setDirectionMode(11, GPIO_DIR_MODE_OUT);
GPIO_setPadConfig(9, GPIO_PIN_TYPE_STD); //MSDI RST
GPIO_setPinConfig(GPIO_9_GPIO9); //MSDI RST
GPIO_setDirectionMode(9, GPIO_DIR_MODE_OUT); //MSDI RST
//
// Initialize the SPI
//
initSPI();
//
// Loop indefinitely
//
while (1)
{
GPIO_writePin(9, 1);
DEVICE_DELAY_US(1000);
GPIO_writePin(9, 0);
DEVICE_DELAY_US(1000);
spi_write(0x1A,0x000000);
spi_write(0x1B,0xFFFFFF);
spi_read(0x1B);
// //
// // Wait until the EEPROM is ready to write data
// //
// while (readStatusRegister() & MSG_STATUS_READY_M == MSG_STATUS_READY_M)
// {
// }
//
// //
// // Enable wirte on the EEPROM
// //
// enableWrite();
//
// //
// // Wait until the EEPROM is ready to write data
// //
// while (readStatusRegister()
// & MSG_STATUS_WRITE_READY_M == MSG_STATUS_WRITE_READY_M)
// {
// }
//
// //
// // Write to the EEPROM
// //
// writeData(EEPROM_ADDR, writeBuffer, NUM_BYTES);
//
// //
// // Wait until the EEPROM is ready to write data
// //
// while (readStatusRegister() & MSG_STATUS_READY_M == MSG_STATUS_READY_M)
// {
// }
//
// //
// // Read from the EEPROM
// //
// readData(EEPROM_ADDR, readBuffer, NUM_BYTES);
//
// //
// // Check received data for correctness
// //
// for (i = 0; i < NUM_BYTES; i++)
// {
// if (writeBuffer[i] != readBuffer[i])
// {
// error++;
// }
// }
}
}
//
// Function to configure SPI A in FIFO mode.
//
void initSPI()
{
//
// Must put SPI into reset before configuring it.
//
SPI_disableModule(SPIA_BASE);
//
// SPI configuration. Use a 1MHz SPICLK and 8-bit word size.
//
SPI_setConfig(SPIA_BASE, DEVICE_LSPCLK_FREQ, SPI_PROT_POL0PHA0,
SPI_MODE_MASTER, 500000, 16);
//
// Configuration complete. Enable the module.
//
SPI_enableModule(SPIA_BASE);
}
//
// Function to send RDSR opcode and return the status of the EEPROM
//
uint16_t readStatusRegister(void)
{
uint16_t temp;
//
// Pull chip select low.
//
CS_LOW;
//
// Send RDSR opcode
//
SPI_writeDataBlockingNonFIFO(SPIA_BASE, RDSR);
//
// Dummy read to clear INT_FLAG.
//
temp = SPI_readDataBlockingNonFIFO(SPIA_BASE);
//
// Send dummy data to receive the status.
//
SPI_writeDataBlockingNonFIFO(SPIA_BASE, 0x0000);
//
// Read status register.
//
temp = SPI_readDataBlockingNonFIFO(SPIA_BASE);
//
// Pull chip select high.
//
CS_HIGH;
//
// Read the status from the receive buffer
//
return (temp);
}
//
// Function to send the WREN opcode
//
void enableWrite(void)
{
//
// Pull chip select low.
//
CS_LOW;
//
// Send the WREN opcode.
//
SPI_writeDataBlockingNonFIFO(SPIA_BASE, WREN);
//
// Dummy read to clear INT_FLAG.
//
SPI_readDataBlockingNonFIFO(SPIA_BASE);
//
// Pull chip select high.
//
CS_HIGH;
}
//
// Function to write data to the EEPROM
// - address is the byte address of the EEPROM
// - data is a pointer to an array of data being sent
// - length is the number of characters in the array to send
//
void writeData(uint16_t address, uint16_t * data, uint16_t length)
{
uint16_t i;
//
// Pull chip select low.
//
CS_LOW;
//
// Send the WRITE opcode.
//
SPI_writeDataBlockingNonFIFO(SPIA_BASE, WRITE);
//
// Dummy read to clear INT_FLAG.
//
SPI_readDataBlockingNonFIFO(SPIA_BASE);
//
// Send the MSB of the address of the EEPROM.
//
SPI_writeDataBlockingNonFIFO(SPIA_BASE, (address & 0xFF00));
//
// Dummy read to clear INT_FLAG.
//
SPI_readDataBlockingNonFIFO(SPIA_BASE);
//
// Send the LSB of the address to the EEPROM.
//
SPI_writeDataBlockingNonFIFO(SPIA_BASE, address << 8);
//
// Dummy read to clear INT_FLAG.
//
SPI_readDataBlockingNonFIFO(SPIA_BASE);
//
// Send the data.
//
for (i = 0; i < length; i++)
{
//
// Send the data.
//
SPI_writeDataBlockingNonFIFO(SPIA_BASE, data[i] << 8);
//
// Dummy read to clear INT_FLAG.
//
SPI_readDataBlockingNonFIFO(SPIA_BASE);
}
//
// Pull chip select high.
//
CS_HIGH;
}
//
// Function to read data from the EEPROM
// - address is the byte address of the EEPROM
// - data is a pointer to an array of data being received
// - length is the number of characters in the array to receive
//
void readData(uint16_t address, uint16_t * data, uint16_t length)
{
uint16_t i;
CS_LOW;
//
// Send the READ opcode
//
SPI_writeDataBlockingNonFIFO(SPIA_BASE, READ);
//
// Dummy read to clear INT_FLAG.
//
SPI_readDataBlockingNonFIFO(SPIA_BASE);
//
// Send the MSB of the address of the EEPROM
//
SPI_writeDataBlockingNonFIFO(SPIA_BASE, (address & 0xFF00));
//
// Dummy read to clear INT_FLAG.
//
SPI_readDataBlockingNonFIFO(SPIA_BASE);
//
// Send the LSB of the address of the EEPROM
//
SPI_writeDataBlockingNonFIFO(SPIA_BASE, (address << 8));
//
// Dummy read to clear INT_FLAG.
//
SPI_readDataBlockingNonFIFO(SPIA_BASE);
//
// Read the data from the EEPROM
//
for (i = 0; i < length; i++)
{
//
// Send dummy data to receive the EEPROM data
//
SPI_writeDataBlockingNonFIFO(SPIA_BASE, 0x0000);
data[i] = SPI_readDataBlockingNonFIFO(SPIA_BASE);
}
CS_HIGH;
}
void spi_read(uint32_t address)
{
uint32_t recieve_buffer = 0x00;
uint16_t registers[2];
uint32_t send_data = (0x00000000 | (address << 25));
for (i = 0; i <= 31; i++)
{
if (((send_data >> i) & 0x01) == 1)
{
parity++;
}
}
if (parity % 2 == 0)
{
send_data = send_data | 0x01;
}
registers[0] = send_data >> 16;
registers[1] = send_data;
GPIO_writePin(11, 0);
SPI_writeDataBlockingNonFIFO(SPIA_BASE, registers[0]);
SPI_writeDataBlockingNonFIFO(SPIA_BASE, registers[1]);
rx_buff[0] = SPI_readDataBlockingNonFIFO(SPIA_BASE);
rx_buff[1] = SPI_readDataBlockingNonFIFO(SPIA_BASE);
GPIO_writePin(11, 1);
recieve_buffer = ((recieve_buffer | rx_buff[0]) << 16 | (rx_buff[1]));
recieve_buffer = recieve_buffer >> 1;
parity = 0;
}
void spi_write(uint32_t address, uint32_t data)
{
uint16_t registers[2];
uint32_t send_data = (0x80000000 | (address << 25)); //31st bit should be 1,address should be on bit 25-30
send_data = (send_data | (data << 1)); //shift whole data to 1 bit left, because on bit 0, there is PAR (parity)
for (i = 0; i <= 31; i++)
{
if (((send_data >> i) & 0x01) == 1)
{
parity++;
}
}
if (parity % 2 == 0)
{
send_data = send_data | 0x01;
}
registers[0] = send_data >> 16;
registers[1] = send_data;
GPIO_writePin(11, 0);
SPI_writeDataBlockingNonFIFO(SPIA_BASE, registers[0]);
SPI_writeDataBlockingNonFIFO(SPIA_BASE, registers[1]);
GPIO_writePin(11, 1);
parity = 0;
}
//
// End of File
//