This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
we are looking for a USB current limit device that could tolerate 10V at VBUS, since they have met VBUS transient that break the USB current limit device. And during the surge test, the TVS on VBUS could clamp VBUS below 10V.
We have proposed this device, which is somehow overspec since we don't need other features integrated in this device.
The customer asked why we design this device with so high voltage tolerance? what's the target application case that VBUS could face voltage as high as 30V?
And do we plan to release lower voltage device?
Hi Howard,
The battery voltage range of VBUS would be 4.5-36V for soft-start and load dump. Thus, if need VBUS short to battery, this feature should be good.
I am confused what device do you need? just for current limit?
Best regards,
Ansel