Part Number: DS90UB954-Q1
Other Parts Discussed in Thread: ALP, USB2ANY
Hi TI support team
About 953&954 mode setting for non-sync CSI mode.
From TI application notes: snla267 page 5: On the 953, register 0x03 controls MODE_SEL after power up and On the 954, register 0x6D bit 1:0 can be controlled for FPD3_MODE (00: CSI Mode)
Because 953&954 mode strap pin can setting by resistor and also control by register.
Because configuration of the FPD-Link III operating input mode may be done through the MODE input strap pin, or through the configuration register bits.
So my question is that when mode strap pin setting as sync CSI mode from HW design but SW can re-configuration to non-sync mode with below register. Is it correct ?
DS90UB953 : register address 0x03 value change to 0x5A
DS90UB954: register address 0x58 value change to 0x5A; register address 0x6D value change to 0x7C;
Can you please let me know if i have missing some other register ?
Thanks
Yutai