Part Number: TMDS181
Hi,
I'm encountering some troubles with the TMDS181.
I use this device in order to create an HDMI input which is connected to a FPGA (Zynq US+)
The output waveforms are not correct, I have some kind of de-emphasis, see below:
I'm using I2C configuration, I didn't modified the default values.
I also tried pin strapping mode, it didn't changed anything.
I always have the same issue whatever the bitrate I use.
Here's the schematic:
Thanks,
Pierre.