Part Number: DS90UB941AS-Q1
Customer confused that “For splitter mode with external REFCLK, the most basic option is to use REFCLK0 = PCLK0 and REFCLK1=PCLK1.”in 941AS datasheet, however,datasheet also describes that "only in independent 2:2 mode,you can configure REFCLK0 = PCLK0 and REFCLK1=PCLK1“,then in single DSI split screen condition, how to configure REFCLK0 = PCLK0 and REFCLK1=PCLK1?target purpose is that it can configure REFCLK0 & REFCLK1 up to105M, to support per port .
BTW,customer thinks that, clock mode is 01, the mean is External Reference Clock Mode, then according to 0x3e,0x3f description,put external clock in fractional frequency at least 2 fractional frequency,the mean is REFCLK0 = REFCLK1 = 210M, then according to fractional frequency, per port pclk up to 105M, in this condition, external input clock should be configured to a maximum of 210M. Is it right ?