Hi Team,
I would like to check below connection. 941+948(dual lane)
1. internal pattern generation with external clk, where should I connect the external clk? DSI0_CLK or DSI1_CLK?
2. REFCLK0/1 short to GND if I dont use splitter mode, is it correct?
3. internal pattern generation with internal clk, Could DSI0/1_CLK leave floating? or they should connect to GND only?
4. If I use VDDIO=3.3V to let I2C operate in 3.3Vmode. Does it mean that GPIO's VIH, VIL is followed by 3.3V condition? Any other connection should be concerned?
Roy