Part Number: DP83867E
Dear TI support,
Observation: DP83867E is not able to establish Ethernet link in 100BASE-TX mode if an IEEE non-compliant link partner has +280 PPM stable frequency offset (typically 25.007089 MHz).
Question: Is it possible to tweak DP83867E, possibly by software means via register access, to be able to establish reliable 100BASE-TX Ethernet link to the IEEE non-complaint link partner with the inaccurate oscillator having the constant frequency offset (+280 ppm)?
Reproducibility: It is possible to use an evaluation board DP83867ERGZ-S-EVM and the non-compliant device to reproduce the observation. On the other hand, PHYs by other vendors we have tested can accept the +280 PPM link partner clock frequency offset.
Rationale: We need to integrate our devices with DP83867Es into an existing customer infrastructure. In the existing infrastructure there is a bunch of non-compliant devices with the inaccurate oscillator mentioned above. We cannot repair the customer's devices and we are supposed to solve the issue on our side with DP83867E.
Thank You,
Cyril