I intend to connect 4 cameras to a processor over Serdes. Here I am adding 2 solutions for Deserializer.
Solution #1: Using 2 DS90UB954 ---> multiplexer. ----> MIPI CSI ---> PROCESSOR
Solution #2: Using DS90UB960 ---> PROCESSOR
The difference from Solution #1 to Solution #2 is the deserializer part number and the multiplexer. My processor can support only 1 MIPI CSI port. Want to understand from you if the Solution #1 would be feasible technically? The data rate for the Camera in less than the supported data rates of the devices.