Part Number: TPS25750
Other Parts Discussed in Thread: BQ25731, TPS55288
Hi,
We need to support some PD adpater project, some with PPS source requirement that we can't support, but we can use TPS25750D to support non-PPS_Source project.
The PDO requirement is as below which looks ok to us.
- PD 24W 5V 3A, 9V 2.67A, 12V 2A
- PD 27W 5V 3A, 9V 3A
My question is, what's the major difference if we choose TPS55288 or BQ25731 (on TPS25750D EVM). Can you provide some explanation about this?
THanks,
Antony