Part Number: DS90UH940-Q1
Hello, Team,
In Table Output State (datasheet p24), it is stated that "CSI-2 OUTPUT" should be "HS0" when "SERIAL INPUT"="Static" (no input signal), "PDB"="H", "OUTPUT ENABLE"="H", "OUTPUT SLEEP STATE SELECT"="H" (5th row).
When tested using an actual device, the mipi output was ~500mV (i.e. neither LP mode nor HS mode) which does not match with the datasheet.
1. What do you think is causing this mismatch?
2. Is there any other missing conditions which might be causing this?
Thanks and Best Regards,
Masaru Oinaga