Part Number: TPS25830-Q1
Hi
could you tell me if TPS25830 (USB 2.0) can compatible with USB 3.0? meanwhile include 5V/3A function.
Do we have any other hero device to recommend? thank you!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS25830-Q1
Hi
could you tell me if TPS25830 (USB 2.0) can compatible with USB 3.0? meanwhile include 5V/3A function.
Do we have any other hero device to recommend? thank you!
Hi Pei,
The part can't be compatible with USB3.0. You should add other device to support the USB3.0 communication.
I am not sure about the USB3.0 communication device.
The part can support type-c which is 5V/3A charging.
For TI's policy, I will first click resolved button.
If you have any other concern, contact me any time.
If you think resolved, please help click 'Issue is solved button'.
Thanks.