This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83849I: Maximum internal clock frequency

Part Number: DP83849I

Hi Experts,

25MHz external clock source is used for DP83849. This clock is used to generate 125MHz internal clock. Is this 125MHz clock the maximum frequency within this PHY which is 5 times by PLL? Or does PLL generate higher frequency?

This is required to make EMC document.

Regards,

Uchikoshi