Part Number: DP83848I
Hi,
LED LINK is glowing , LED ACT is not glowing
Voltages are monitored at RBIAS - 1.2v, PFB pins - 1.8V
can you help me please.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DP83848I
Hi,
LED LINK is glowing , LED ACT is not glowing
Voltages are monitored at RBIAS - 1.2v, PFB pins - 1.8V
can you help me please.
Hello,
To double check link LED, does register 0 also confirm link is established while LED LINK is glowing?
What is LEDCR Register 0x18 reading? Does this confirm LED LINK and LED ACT mode is set as expected?
Thank you,
Nikhil
Hello,
There are 2 problems.
First: The RBIAS must to be 4,87k1% instead of 4,7k.
Second (probably the main): The MDI_TN signal is connected to the TCT pin of RJ45 and the MDI_RP signal to the RD- pin of RJ45.
Try jump those signals with short wireups.
Jagher