Hello,
May I know the difference between 953/935/951?
Can I replace it each other without any modification in register's setting?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
May I know the difference between 953/935/951?
Can I replace it each other without any modification in register's setting?
Thanks.
Hello Ryan,
It depends about your use case and used settings.
Basically the 953 and 935 can be replaced 1:1.
But the 951 has some differences:
951 Supports only Non-Synch Mode.
Supports only a fixed forward channel rate = 4.85Gbps. Hence, it is not compatible with the 954 or 936.
Hi Hamzeh,
Thanks for your information.
Dose "951 supports only non-sync mode" mean that the clock source must locate at serializer CLKIN?
Regards,