Part Number: DS90UB935-Q1
Dear team,
My customer wants to know whether our device 935&960 can pass through embedded line?
For example, camera's resolution is 1280*720 which means that line count=720 and line length=1280. In order to achieve functional safety, they need to add one line at the end, and this line's name is embedded line. This line will include some diagnostic information. This line comes from ISP, and this line needs to be passed through to SOC, then SOC analyze the embedded line.
In my understanding, our device can support such passthrough function only if ISP sets line count=721 and SOC sets line count=721 at the same time, right?
Thanks & Best Regards,
Sherry