Part Number: TPS65987D
Other Parts Discussed in Thread: TPS25750
Hi Team,
We have some questions regards to TPS65987DDH. Hope you can help to advice, thanks in advance.
We are using this in our first USB-C PD design on a portable wireless printer. At first it will be configured as a simple UFP sink. Later we may support power output to charge a smartphone. We are also evaluating this IC for use in USB-C updates across a number of portable printers.
In terms of configuration I need to negotiate a power contract with sufficient power to print or take the max available. 5V 3A isn't quite enough, but 9V >2.85A (about >25W) and so on at higher voltages is sufficient to print. It can accept 5-20V input.
Here are a number of questions I have regarding programming this IC.
- Is any configuration register data retained between power cycles?
- The parts on my prototype board have out-of-date firmware. Its F707.10.00 and the latest is F707.10.08. Is updating the IC's application code required or recommended? Is there any example code or how-to for this? I think I understand how to do it using the "Patch Bundle Update" tasks in the programming guide. But that's a lot of work just to load the latest FW. Is there any possibility of buying the IC with the latest FW loaded loaded?
- The config tool is helpful but it doesn't expose settings for all registers. In some cases it doesn't quite match the host interface guide. Should I give precedence to the tool or the programming guide?
- When I "save binary" what is in the image? Does this include the register settings and the latest FW binary? Then do I load this through the "Patch Bundle Update" tasks? Is this a one-time operation, all the settings are permanent? How are most designers using this part?
- The "AutoNegotiate Sink" register (0x37) seems key to negotiating the required power. However the config tool doesn't expose most of the setting in the upper bytes. Not sure how to approach this. What is the interplay between this register and the Tx sink capabilities register?
- In a number of places the tool writes 0b1 to reserved bits. For example in the 2nd byte of register 0x37. Does this matter?
Thanks and regards,
Don