This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN1043-Q1: is there alternative part for TJA1145T?

Part Number: TCAN1043-Q1
Other Parts Discussed in Thread: TCAN1043

Customer is looking for the replacement for TJA1145T, but TCAN1043 does not have the SPI feature. Could you please help further check it? Thank you.

  • Hi Aki,

    Our equivalent device would be TCAN1145. There are two other variants, TCAN1144 and TCAN1146, which offer different feature sets. See page 3 on the datasheet for a feature table of these three devices.

    Note that while these are all pin-to-pin compatible with TJA1145T, there are some register differences between this and TCAN114x's. 

    Regards,
    Eric Schott