Part Number: DP83867IS
Question1:
Is the only difference between two-supply and three-supply operation the power consumption?
Question2:
Does the device have an integrated LDO that drops the 2.5V rail to 1.8V for certain internals? (this is why two-supply has larger power consumption?)
If not, what voltage do the internals, that run at 1.8V with external 1.8V applied, run at, when the device is operated in two-supply mode?
Question3:
When operating in two-supply mode, does anything register/setting-wise need to be changed? Or do you simple just need not power the 1.8V pin?
I did a quick check on the DS and didn't see anything, but I might have missed something.
My customer doesn't have experience with two-supply mode, and needs to do some risk assessment before switching.
Thanks!
Darren