Part Number: LM8335
Other Parts Discussed in Thread: TCA6408A
Hello
Is the LM8335 available a Extended register read & write?
If available, How to use it?
Best regards.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Louis,
The LM8335 does not support read access, so only extended writes are supported.
Regards,
Eric Schott
Hi Eric, Thank you for your reply.
If LM8335 does not support register read, is there another part that supports extended register write, register write/read and we can buy EVB?
that will be a great help to me.
Thanks in advance.
Lui
Hi Lui,
It sounds like being able to read to and write from registers are requirements for your design. We don't have a pin-to-pin compatible device that also offers these features, so I'd like to know the other requirements you have to best recommend a suitable device.
In general, I would recommend TCA6408A as an 8-bit I2C I/O expander. This device supports both reads and writes to its registers (writing so the input state registers has no effect) and is operational in the same supply range as LM8335.
I would encourage you to check out our I/O expander product page. Here you can sort through our devices to find which ones meet your needs. If you have specific questions about any device that you can't find on the datasheet, you can ask about them here.
Regards,
Eric Schott
Lui,
Can you elaborate a bit more on what is needed? We don't have another general purpose IO expander device with extended register writes or reads, but we have some I2C IO expanders with limited extended register writes and reads.
Regards,