This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65981: schematic check

Part Number: TPS65981

Hi 

1.could you help check the TPS65981 schematic as below and any need to adjust ?

2.In addition, the 12V voltage transmitted from TPS65981 will be used for the entire circuit board.
Can the 12V main power supply be controlled by an external button to turn the power on/off?

USB PD_TPS65981.pdf

  • Hello,

    1. The power path for the TPS65981 is correct with the required capacitances.

    2. Can you please elaborate on your question? Do you want the TPS65981 EVM to sink 12 V to another application?

    Thanks,

    Mike Emanuel

    Please click "Resolved" if this answered your question.