Part Number: TUSB8041
Hello,
I have manufactured design TIDA-00288, but it isn't fully operational. After plugging it into a computer, I have taken a multimeter to check the 5v, 3v3 and 1v1 rails and they all look good, but the computer isn't detecting it as a USB hub. This design uses the TUSB8041, so this is the center of my focus. One anomaly I have found is that Pin 50, GRSTz, has about 3.3V on it. I have confirmed it isn't shorted to the 3v3 rail, so I'm not sure where it's coming from since it is connected only to a capacitor and then to ground.
I have made 3 minor modifications to the TIDA-00288 design. First, I only needed 3 downstream ports, so the fourth one is not being used. Second, I changed the downstream ports from the USB 3.0 A connector to USB 2.0 Micro. This has left the TX and RX pairs unused, so I am only using the D+/- for data from the downstream ports to the TUSB8041. I have left the TX and RX pairs connected to the upstream port, because this connector was left unchanged. Third, I added 4 low power LEDs to the 5v rail. They draw 0.4mW each, which Art Mecina of TI had confirmed would be safe to add (Thanks again, Art!).