Other Parts Discussed in Thread: TCAN4550
I am trying to connect to a classical CAN Bus using the TCAN4550EVM, but I am not receiving a CAN message.
I got the version of the board I am using with SPI, but it is 3.2.1 from the following.
address:0x1000 value:0x32150320
address:0x1004 value:0x87654321
The specification says "• Classic CAN Backwards Compatible", so I think I can connect.However, I have not been able to receive the Classical CAN message.
I downloaded TCAN4550 Demo Software and tried to send a message from Kvaser's USB CAN I / F with FDOE of Control Register set to 0, but the reception process does not work.
When receiving in a classical CAN environment, is there a place other than FDOE to change the setting to CAN FD?