This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83TD510E: Board layout for termination circuit

Genius 17405 points
Part Number: DP83TD510E


Hello,

My customer has an question for the board layout related to termination circuit.
The datasheet says that “Differential traces must 100-ohm differential”.
Because of pin layout of RX+, RX-, TX+ and TX-, to prioritize differential traces of RX pair and TX pair, some vias have to be used for board layout.
Aactually our EVM uses some vias.

I just confirm the priority.
The 1st priority is keep differential trace of each pairs, then minimum vias that could change the impedance is acceptable.
Is this understanding correct?

Regards,
Oba