Part Number: TCA9617B
Other Parts Discussed in Thread: INA228, TCA9800, TCA9803, TCA9509
Hi,
We are using TCA9617B as bus repeater. We have 7 devices on B side and these are IN228 current sensors.
The SCLB output of TCA9617B is specified to maintain a static offset voltage of 0.5V while driving LOW which is understandable as per datasheet.
But the INA228 device specifies a VIL max of 0.4V.
How can we make sure INA228 device detects the LOW level signal driven by TCA9617B on SCLB / SDAB correctly?
Regards,
Manjunatha