Part Number: DS90UB960-Q1
I plan to use the 960 with four 1080p cameras that will all be synchronised. I plan to use two CSI ports to send two cameras each. I have some questions.
1. Will the video data from each port arrive approximately at the same time? I want to have something like below with the lines arriving together give or take a few pixels.
Line 1 - CAM1/2, Line 2 etc
Line 1 - CAM3/4, Line 2 etc
I plan to have it so that the lines of the two cameras are concatenated together
2. If I removed one of the cameras (lets say 1) then would I just get cam 2 sent, or would the port just send some dummy data rather than the camera one data? If possible I would prefer that it still sent something.
Thanks
Jon