This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65DP159: Is it possible to swap input Polarity for D2 pin only?

Part Number: SN65DP159

My customer is asking me following and please kindly checkout my estimated answer below?

Q1 s it possible to swap the polarity of only the D2 pin on the output side of the SN65DP159?
     My est ans: No. All inputs n - p will be swapped. it cannot control only for D2 pin.

Q2: it possible to swap the polarities of both input and output only for the D2 pin?
     My est ans: No. Output lanes never change. It will only change input lanes.