This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UH940-Q1: Preferred procedure for the clock lane output to follow mipi standard

Part Number: DS90UH940-Q1

​Hello, Team,

The device is DS90UH940-Q1.

The customer would like to know the preferred procedure of how to set resistors in order to start a clock lane output which follows the mipi standard.
If there is any document that demonstrates it, it would be very much welcomed.

Thanks and Best Regards,
Masaru

  • Hi Masaru,

    Could you clarify what you are looking for? You shouldn't need resistors on the clock lane.

    For register settings, as long as data is sent to the 940, the 940 will output data and clock following mipi standard.

    Best Regards,

    Charley Cai 

  • Hello, Charley,

    The customer's setting cannot always confirm that the input signal exists at the power-up of 940.
    Therefore, they are doing digital reset after setting the initial values to the register and inputting video.
    This is according to the description given in the datasheet p90 note (1), and I believe this is required for a pairing with the Serializer.

    After the digital reset, the output sequence should follow the mipi standard; correct?

    Thanks and Best Regards,
    Masaru

  • Hi Masaru,

    Yes, the digital reset is to ensure the 940 will lock to correct video stream. After the reset, the DSI output will follow mipi standard. 

    Best Regards,

    Charley Cai