Part Number: TNETE2201B
Dear Technical Support Team,
When specific data is received, 62.5MHz clock waveform supplied by RBC0 continues abnormally.
At this time, K28.5 is input regularly, however SYNC doesn't show High (SYNCEN is enable).
This issue is not always occurred(sometimes occurred).
When change LCKREFN such as high → low → high, a correct 62.5MHz clock was output and SYNC was also high.
So I guess that CDR doesn't lock during SYNC issue.
■Received pattern for SYNC
TNETE2201B is received following pattern continuously.
/K28.5/D21.5/D0.1/D0.0/ or K28.5/D2.2/D0.1/D0.0/
■Behavior about RBC0
When a problem occurred, it was confirmed that after outputting a normal 62.5MHz clock for 5 cycles, it was stretched once at the rising edge and once at the falling waveform. After that, this state is repeated
If differential input( K28.5) is nothing , the output clock of RBC0 shifts phase and TNETE2201B stretches the clock of RBC0 just once.
I think this is the correct device spec behavior( Figure 2. Word Realignment Timing Characteristics Waveforms on datasheet) for K28.5 character detection.
■Questions
①Is this RBC0 expected behavior(stretched clock twice) as a device when SYNC hasn't been high and CDR hasn't been locked?
②Have you ever seen this SYNC and RBC0 issue?
③Please investigate the route cause of this event and confirm its ripple.
For example , does it occur issue other than the Autonego code (/K28.5/D21.5/D0.1/D0.0/ or K28.5/D2.2/D0.1/D0.0/) ?
Best Regards,
ttd