Part Number: TIOS1013
Dear team,
The customer are considering dual mode load operation. They want to connect NPN type and PNP type load same time.
Is there any solution like 2ch output type of TIOS1013?
Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Dino,
The TIOS1013 is capable of working with both NPN and PNP applications. But currently there is not a 2-channel version of the TIOS1013. The customer would need to implement two TIOS1013 devices if they wanted to implement both an NPN and PNP solution at the same time.
Regards,
Jonathan