Part Number: TS3USB30E
Hi,
looking at the corresponding datasheet there is a confusing information:
It says: "Power to the device is supplied through the VCC pin and should follow the USB1.0, 1.1, and 2.0 standards."
As I understand the 5V of USB should be applied.
But at Section 6.3 recommended power supply is 4.3V as maximum.
What´s right? Do I missunderstand the mentioned sentence or is it incorrect?