Part Number: DS26LV31T
Dear Team,
My customer wants to use DS26LV31TM/NOPB on a non-ROHS soldering process. they would like to know if the part is backward compatible.
Could you please help on this?
Best Regards,
Caglar
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS26LV31T
Dear Team,
My customer wants to use DS26LV31TM/NOPB on a non-ROHS soldering process. they would like to know if the part is backward compatible.
Could you please help on this?
Best Regards,
Caglar
Caglar,
I think it depends on the soldering process. Here I copy TI standard reply for all soldering profile questions:
• At the board level, solder reflow profiles are dependent on numerous factors including, but not limited to, solder type, flux, package type, number of components, board layers, board size, reflow oven type and accuracy as well as pre and post cleaning processes. Because of the number of variables it is not possible to provide a single reflow profile that is representative of every board using a specific package type. Typically manufacturing houses have reflow profiles in place and modify them for specific hardware.
• TI suggests using the flux manufacturer’s recommended profile as a starting point. In general ceramic parts are compatible with ramp-rates of less than or equal to 5°C/second with a maximum temperature of 265°C. Variations of course need to be comprehended based on time required to volatize the flux prior to the solder reaching liquidus.
• Metal lid packages use a 80%Au20%Sn gold-tin solder preform to attach the lid. Gold-tin solder will begin to soften at 270°C and has a eutectic point of 280°C. The package body temperature must not be allowed to exceed 265°C at any time or permanent damage will occur due to compromising the package’s hermetic seal. Note that though-hole hermetic device specify a maximum temperature for soldering as a lead-temperature of 300°C for 10 seconds. This is not a reflow temperature.
• When using gold-plated leads or pads with MIL-SPEC plating thickness (60 µ-in to 225 µ-in), it is strongly recommended that the units be pre-tinned (solder-dipped) before board mounting to scavenge the gold from the leads or pads. If this is not done there is a chance of gold-embrittlement of the board-level solder-joints. A flowing solder-pot or two passes in a static solder-part is recommended.
Hopefully it's helpful.
Regards,
Hao