Part Number: DS90UB934-Q1
Hi team,
fdev is specified as +/-0.5% to +/-2.5% at 25 to100MHz
fmod is specified as 5 to 50kHz at 25 to 100MHz.
Could you advise the fdev and fmod at PCLK = 74.25MHz?
SSCG_MOD_RATE register describes as frequency modulation PCLK/3168 +/-1%
74.25MHz/3168 = 23.4kHz +/-1%
Is this modulation frequency?
Or 23.4kHz is the modulation frequency and +/-1% is the deviation?
deviation frequency also changes by PCLK?
regards,