Part Number: DP83822I
Hi,
I wanted to know if the Halo HFJ11-E2450E model can be used with the DP83822I.
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DP83822I
Hi,
I wanted to know if the Halo HFJ11-E2450E model can be used with the DP83822I.
Thanks
Hi Bottini,
Section 11.1.3.1 of the datasheet provides a table of specifications for the transformer. As long as the transformer you use aligns with the specifications, it should work. In the HFJ11-E2450E datasheet, it seems only return and insertion loss are listed. In order to get the other specifications and see if the transformer would be compatible, you would need to ask the vendor to provide it, along with the tolerances. We typically recommend a tolerance of +/- 2%.
Regards,
Adrian Kam