Other Parts Discussed in Thread: TUSB2077A
I made a hub with the TUSB2077, but it is not recognized by a host using ISP1504 ... is that right?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TUSB2077A
I made a hub with the TUSB2077, but it is not recognized by a host using ISP1504 ... is that right?
Hello Gabriel,
What are the symptoms of the non-working hub? Is it enumerated? Are the downstream devices recognized? Does it got enumerated and then it crash? etc....
Regarding the schematic, there are a couple of thing I would like you to try:
1) You are using the TUSB2077 in the GANGED mode, so all the OVRCUR terminals must be tied together, in addition I recommend pulling them up through a 15K resistor.
2) Place a 22pF capacitor to Gnd on the DP0 and DM0 terminals, in addition, I can't see in the sch if there is a 30 ohm series resistor on DP0 and DM0, if not, place them.
3) For the RC circuit you are using for resetting the TUSB2077, make sure the values of R# and C# are so that make a 1.5 to 2 ms long pulse (a 20K with 1uF is recommended)
4) The capacitors network shown in your schematic (C4 to C33) are placed backwards, perhaps is just matter of the symbol you are using in your schematic but is worth to check that.
If you can tell in more detail what is the failure like, it will be very helpfull.
Regards.
I am using only part of the hub, the rest of the circuit of the file was not mounted yet.
The hub has been tested on several PCs and it worked perfectly, but to turn it into a pci to usb host ISP1504 has one, it is not recognized, this card runs Angstrom Linux, and the manufacturer told me that type devices keyboard, mouse and TUSB2077 not work in this host, I found odd and decided to ask directly to the staff of Texas (you guys), according to them is that the host and the hub is 2.0 is 1.1 ...
Hello Gabriel,
The fact that the host is USB 2.0 compatible and the TUSB2077 is USB 1.1 compatible will not cause tha hub to stop working. USB 2.0 is fully backwards compatible with USB 1.1 specification.
If your hub configuration is working on another systems, then a host side issue is more likely.
Can you check the integrity of the signals DP/DM going from the host to the TUSB2077? (differential impedance, swing voltage,etc.)
You can check the section 7.1 of the USB 2.0 specification for signal compliance.
Regarding to the Angstrom, any operating system that has native USB stack support should include a HUB driver as part of that stack.
Regards.
Hi Gabriel,
You need to contact NXP to check the capabilities of the ISP1504 for supporting full speed and low speed devices. Some OTG tranceivers have limitations when implementing them as a USB host.
Make sure that the ID pin of the ISP1504 is set correctly.
Regards.
Hello, Elias
Thank you so much attention, but unfortunately the TUSB not work, I made a new layout using the uPD720114 and is working perfectly