This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS25BR110: Theta JB Thermal resistance for DS25BR110TSD/NOPB

Part Number: DS25BR110


Hi Team,

Can you tell me the Theta JB Thermal resistance for DS25BR110TSD/NOPB  package if this is available?

Thanks,

Jonathan

  • Hi Jonathan,

    Junction to board is not available. This is because this depends on the board material and heat dissipation. Having said this, we can calculate maximum junction temperature.

    Device draws 43mA - maximum. With worst case supply - 3.6V - this means we are drawing about 150mW. With Theta JA of 60 degC/W, it means junction temperature would about 9.5DegC higher than ambient. At maximum operating temperature of 85degC, this means worse case junction temperature would be at 85+9.5 or 94.5degC.

    Regards,, Nasser