Part Number: TUSB1046EVM
Hello,
I tried to display 5K video on the display with USB Alt DP using TUSB1046EVM, but it doesn't work.
The details are as follows. Can you guess what is the cause?
INPUT: 5K60Hz video, DP1.4 (output from PC)
OUTPUT: USB Alt DP (input to display under development)
■ Occurrence phenomenon
◇The display has no screen display *The Display I am using is for 5K only, which may be the cause
◇On the PC setting screen, FHD output is displayed
◇Resolution change not accepted from PC
Is it possible to output 5K60Hz video as the performance of this evaluation board?
If possible, why do you think this is happening?