Part Number: TUSB542
Hi team,
My customer is evaluating the TUSB542 with following configuration.
The reason for this is unknown, but we are experiencing USB communication loss within a few minutes. We have used the above processor and a conversion adapter from another company in past models (not equipped with TUSB542), but the communication never disconnected (about 10 hours).
Question.1
As a redriver setting
The setting of (CNFG_A1, CFNG_B1) = (High, Float) remains the same.
(CNFG_A2, CFNG_B2) = (Float, High) setting A and
(CNFG_A2, CFNG_B2) = (Low, High) setting B
Then, the jitter changes with the RX signal on the processor side.
What is the factor that changes the jitter due to the difference in the above parameters?
Question.2
In the example circuit in the datasheet (Figure 16), there is no bypass capacitor for the power supply. How much capacitance should I connect to the bypass capacitor to avoid worsening the jitter?
Question.3
As mentioned above, it seems that there is sensitivity to the occurrence rate of the disconnection phenomenon by changing the parameter settings on the RX side. By the way, does the behavior on the TX side affect the RX signal?
Regards,
Yamaguchi