Part Number: DS90UB954-Q1
Hi Team,
Can you kindly support with the the device parameters :
1. In my design, I would like to supply the VDDIO with 3.3V
a. would the CSI levels be referenced to the 3.3V or would they be referenced to VDD18_CSI voltage levels?
b. Can the PDB pin be directly connected to the 3.3V rail GPIO ?
c. With this voltage at VDDIO, would the voltage levels at the RN0/1 be 3.3V ?
2. What purpose does the GPIO serve at the deserializer ?
a. In my design I do not have sufficient GPIO lines available and hence would like to know if this is critical for any particular use case in a camera applicaiton
3. I would like to use the 2MP/60FPS setting for the device? Can you please help me understand what should be the configuration on the MODE pin?