This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCA9535: Package information of SSOP (DP)

Part Number: TCA9535

Hello team,

I have a request regarding package information.

The datasheet said SSOP package has 24 pins. However, for "Mechanical data" in the datasheet, the information of 28 pins package is mentioned.

Can you send me the correct data? I searched it on the TI.com, but I could not find it.

Best regards,

Shotaro

  • Hello Shotaro,

    The picture used in the mechanical drawing is just a general image for modeling the IC. If you notice on the bottom table the dimensions change based on what variant you select. Since this IC comes in the 24 pin variant the dimension of A would be between 8.5 and 7.9 mm.

    The rest of the dimensions are the same between variants.

    Best,

    Chris