Hi Team,
There is TPS25750S and TPS25750D and the difference is the following.
TPS25750D: high-voltage integrated source path, 4 x 6 mm QFN package.
TPS25750S: uses an external NFET power path, 4 x 4mm QFN package.
Is there any criteria to select these two devices?
For example, TPS25750S is recommended when the application is more than 60W, etc.
Best Regards,
Yaita