Part Number: TUSB320
Hello Team,
My Customer is planning to use the TUSB320 in his design. However, needs to clarify few things:
Regarding pin VBUS-DET:
According to the datasheet, there shall be 900k to VBUS. But if VBUS is 5V the level of VBUS-DET is below the threshold level of VBUS-DET which is >2.9V.
Shall I use 50k if the VBUS is 5V? Or will they get a detection despite the level is below the threshold?
Regarding pin ID:
They have tried to set pin PORT to high, low and Not connected. But the ID pin will not turn low.
They have connected the USB C connector to a PC using a USB C - USB C Cable and a USB C to USB Type-A Cable.
Regards,
Renan