Part Number: TUSB1044
Hello,
Can a single TUSB1044 be used in a USB C receptacle to USB C receptacle application with full feature function? If so, are there any app notes or reference designs demonstrating this?
Thanks,
Michael
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TUSB1044
Hello,
Can a single TUSB1044 be used in a USB C receptacle to USB C receptacle application with full feature function? If so, are there any app notes or reference designs demonstrating this?
Thanks,
Michael
Michael
You can't as this design will potentially extend the USB Type-C cable to more than 1m which is a USB spec violation. Having the two Type-C receptacles on both ends will also create issue with Normal and Flip orientation configuration.
If you want to design with USB Type-C receptacle on both ends, you need a hub in the middle which is a Type-C dock design.
If you only want to use the TUSB1044, you have to design with a Type-C plug on one end and then a Type-C receptacle on the other end.
Thanks
David