Part Number: TUSB9261
Hello Support,
Can someone point to the latest information to make a flash burner for Linux?
The user guide (and code) that can be found on this forum is dated 2013, and the procedure one has to follow doesn't work (libs not not exist anymore, compilations fail...).
Or better, just an installer ... I'm a HW guy, not a SW guru, please accept my apologies.
FYI, we're using a Nvidia SOM Xavier on our PCB, and this SoC doesn't have a SATA interface (even if the TRM says so..., marketing!). The Jetson devkit is using a Marvell PCIe-2-SATA bridge, but Marvell doesn't sell the chip if we don't order 10K's units/year and pay a license for using it. We plan to use the TUSB instead, but we need to flash the SPI from the Jetson OS (Ubuntu).
Thank you very much,
any help is appreciated.
ESz