Part Number: TPS65987D
Hi Team,
I plan to use TPS65987D in the following configuration :
PP1 switch: Sink only, PDO1
PP2 switch: Souce only (5V, 0.9A)
PP3 switch: Sink only , PDO2, PDO3, PDO4,
Sink PDO-s:
PDO1: 5V, (12W)
PDO2: 9V, (12W)
PDO3: 15V, (12W)
PDO4: 20V, (12W)
My question : is it possible, and if yes, how to achieve this with the application customization tool ?
Thanks,
Zoltan