Part Number: TPS65987D
Other Parts Discussed in Thread: TPS65988, , TPS25750
Hi,
Currently, I bought the USB-C-PD-DUO-EVM and the TPS65988 EVM. I want to make the USB-C-PD-DUO-EVM source board to supply power to the TPS65988 EVM, then TPS65988 EVM as source to provide power to the sink side of the USB-C-PD-DUO-EVM. It will look like the picture below. Is it possible? If yes, how to configure the setting of these two board? Do I need to change the firmware of them? And if I want to change the USB-C-PD-DUO-EVM to maximum power 200W, how to do that? I change the sink and source capacity from the software, but it did not work.
Best,
Rex