This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB8041: USB Upstream Signals control into TUSB8041

Part Number: TUSB8041

Hi Expert,

The engineer has below questions of TUSB8041 applicant.Pls help to comment.

1)Could we control PWRCTL1/BATEN1 by USB Upstream Signals?

2)Could we disable/enable USB Downstream Signals  by USB Upstream Signals?

Best regards,

Eric Lai

  

Field Application Engineer

Texas Instruments Taiwan Limited

O: +886-2-2175-2582

M: +886-909-262-582

E-Mail:Eric.Lai@ti.com  

  • Hi Eric,

    The USB hub switches on and off power to the hub ports based on USB commands from the host, but these commands are a function of the host driver.

    USB Downstream Ports can be disabled / enabled using EEPROM or SMBUS connected to the hub.

    Regards,

    JMMN