Part Number: SN65DSI83
Other Parts Discussed in Thread: TXB0108, TPS65101, DSI-TUNER
Hi,
I am new on this forum, I used to work directly with an application engineer in the past employment but can't seem to be able to reach any of my old contact. Anyhow, I have started a new schematic capture for a display adapter from a MIPI interface to a LVDS display. seem that the SN65DSI83 is the perfect match for what I need.
I was wondering if someone at TI could help me reviewing the schematic prior entering into layout phase so I have a better chance of success using this IC. I also use a TXB0108 for level shifting since my source if 3.3V and the bridge is using 1.8V supply.
I have inserted the 2 pages related to this function into this message. (the other pages are basically connectors and a TPS65101 for the power sequencing)
Any feedback would be greatly appreciated.
Fred Jutras