Part Number: TUSB1044
Hi Team,
For a USB3 only Source side application, which of the following GPIO configuration should I use? The only difference is on DIR1 and I'm not sure if it's a don't-care for USB3 only applications.
Thanks!
Roy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TUSB1044
Hi Team,
For a USB3 only Source side application, which of the following GPIO configuration should I use? The only difference is on DIR1 and I'm not sure if it's a don't-care for USB3 only applications.
Thanks!
Roy
Roy
Please refer to Table 2 of the TUSB1044 datasheet -> One Port USB 3.1 - No Flip or One Port USB 3.1 - Flip, then you can choose between Source and Sink design.
Thanks
David
Roy
DIR[0:1] is only used to select DP Alt Mode and Custom Alt Mode. Since this is USB only, the DIR does not matter. You can use either configuration.
Thanks
David